1/19/2024 8:01 AM | |
Joined: 10/5/2023 Last visit: 8/23/2024 Posts: 11 Rating: (0) |
Hi! Equiptment: I have started this project with the base from the IOL_READ_WRITE application. and set up the I/Olink master according to the manual, with the changes going from ET200 to CM. When trying to read out the tag i do not get any error message nor ID from the FB. As you can see in the attached image i do get presence, and checking IB5-7 the tag information is also beeing read. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/19/2024 11:02:47New subject after splitting //Tom |
|
Follow us on