4/2/2024 6:42 AM | |
Joined: 3/2/2007 Last visit: 10/28/2024 Posts: 942 Rating: (5) |
Kindly, which type of connectors should we use on the SMC module side? where can we get them? 6SL3055-0AA00-5AA3 , Sinamics S120 sensor moduleSMC10sensor board for evaluation of aresolverwithout drive-cliq cable 6SL3055-0AA00-5CA2 , SinamicsSMC30sensor module for incremental encoder: TTL/HTLor combi-encoder SSI with incremental tracks or encoder SSI without incremental signals/ without DRIVE-CLiQ cable 30 mm overall width |
... thank you ... |
|
4/2/2024 9:47 AM | |
Joined: 10/11/2006 Last visit: 10/30/2024 Posts: 5933 Rating: (815)
|
Hello, because of EMV it is better to use pre-assembled signal cables. |
With best regards, |
|
Follow us on