4/23/2024 8:03 AM | |
Joined: 6/29/2018 Last visit: 4/24/2024 Posts: 17 Rating: (0) |
The sampling rate of the TM41 Output pin is too slow for the task. Default setting were some sampling times at 4000us. How do I set the sampling time of all the involved functions to faster value (best case 125us, at least 1ms)?: 1) r2521[0] CO: LR position actual value, Position Control (Starter view "Actual position value preparation" shows that this block is done with p115[4]. Was 1000us, set it to 250us (which was fastest accepted repetition rate) 2) TM41 p115[0] Sampling time for supplementary functions (set from 1000us to 125us now, after all other setting did not speed up) p3299 Variable signaling function sampling time (set from 4ms to 1ms now, after all other setting did not speed up) 3) TM41 Connector binector converter: What sampling time is this calculated? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/24/2024 04:42:51New subject after splitting Last edited by: Jen_Moderator at: 04/25/2024 09:31:34Headline optimized. |
|
Follow us on