Default Header
(header konnte nicht geladen werden)
8/31/2025 1:05 PM | |
Joined: 8/31/2025 Last visit: 8/31/2025 Posts: 2 Rating:
|
We have been facing the F21 fault in our 6RA22 DRIVE (850 AMPS) , WE HAVE SHORTED THE X1 and X2 TERMINALS ON A2 card to bypass the external pulse signal which results in removing the F21 fault but drive is not giving the command to the motor to run despite 1 being displayed on the card. We have changed the A2 card as well as the A1card but the problem is not resolved. We have checked the entire field system as well as the motor but unable to resolve. Can anyone suggest how to resolve this issue. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/01/2025 11:54:38New subject after splitting |
|
Follow us on