Default Header
(header konnte nicht geladen werden)
8/28/2009 2:38 PM | |
Posts: 3 Rating:
|
what is the ES3?? Is it just a LOGO! that has more capability???? could someoneexplain??? |
8/28/2009 3:02 PM | |
Posts: 173 Rating:
|
Easy one this! Siemens has cought out quite a few people with how they released the -0BA6 version of the LOGO! 1) the 'Standard' LOGO! -0BA6 was released in August 2008 (hey, thats about a year ago!) 2) But at the time it did not support Japanese menu text and characters like they had said they would. They released it with the other 9 language support anyway. 3) The Japanese language support was only released in November 2008 at the SPS/IPC/Drives fair. 4) This version is called the ES3 version (ES = E-Stand, which is German for 'Development Step') 5) You can find out what version you have got by looking on the LOGO! for a small cross with numbers in. The number that is replaced with an 'X' is the E-Stand number. Check out the attached document. 6) Anyway, you need at least LOGO! Soft Comfort V6.1.5 (latest service pack release is 6.1.12= SP2) available from the download pages form the LOGO! website. 7) When you select the target device that you are programming for, you should select the 'Standard' 0BA6 for an E-Stand 2 or earlier, and 'ES3' for an E-Stand 3 or higher (E-Stand 4 has just been released, that is why you need the latest SP2 - it supports some nice littel features and fix-ups!) Cheers Aaaarrggh! (Barbarian for 'Have a nice day!') AttachmentLOGO_E-Stand_18298033.zip (873 Downloads) |
This contribution was helpful to
5 thankful Users |
Follow us on