7/21/2017 11:24 AM | |
Posts: 8 Rating: (0) |
Hi all, We are trying to configure our RF reader with sinumerik 840DSL (720.3 hardware with inbuilt S7300 317 CPU) and following RF components are used . We are using standard library given in the following application example for configuring the RFID. https://support.industry.siemens.com/cs/document/63969277/simple-communication-between-simatic-rf160c-and-simatic-s7-controllers?dti=0&lc=en-US After configuration we are trying to reset the RF160C but its giving error ( error code : 1500). we tried with s7300 standalone PLC also,Result getting same. We assume that error might be the problem with the RF parameters because all the hardware is new. We got only one RFID reader so we left X2 port of RF160C as open, Is there any problem with that?? do we want to terminate the X2 port with a terminator?? It will be helpful if someone share some sample project with S7 300 (step 7). Regards / Alfin Paul ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/24/2017 11:04:30 AMNew subject after splitting |
|
7/24/2017 11:07 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on