Default Header
(header konnte nicht geladen werden)
7/26/2019 9:43 AM | |
Posts: 1 Rating:
|
Hello everyone :) I have an issue with rf180c. I tried to connect the product to beckhoff CX1000 but it looks as it doesn't communicate. I added proper GSD file, it is connected via Profinet card, there is no error with hardware configuration, but when I am sending some parametrized index group, offset and lenght in System Manager there is pop up window wit erro 702 - it means the index group doesn't match. I have tried almost all combination of index group etc. Is there any idea what can I do with it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/26/2019 12:52:14New subject after splitting |
|
Follow us on