8/5/2020 1:24 PM | |
Joined: 4/1/2014 Last visit: 11/5/2024 Posts: 3 Rating:
|
HI did u get the solution for above problem...i am facing same problem, ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_551571 at: 08/05/2020 13:27:02Last edited by: Jen_Moderator at: 08/10/2020 06:31:08New subject after splitting |
|
8/7/2020 7:20 AM | |
Joined: 3/25/2008 Last visit: 9/15/2025 Posts: 224 Rating:
|
SET says which parameter set should be loaded into the drive. if it's GA90FF at 400V then the set parameter is SET 9823 3974 12 in the original, but there is the MM420. you need to change .txt to .dnl Attachment9823-3974-12 04 1x4 400V.txt (852 Downloads) |
This contribution was helpful to
2 thankful Users |
8/9/2020 7:49 AM | |
Joined: 4/1/2014 Last visit: 11/5/2024 Posts: 3 Rating:
|
Thank you for your immediate response, i am using MM440 and 380V do you have set data file for this.i have one SET 9823 3974 71, but it is not working .can you check it what will be wrong or do you have another file Attachment9823-3974-71 00 1x4 380V.txt (933 Downloads) |
8/10/2020 9:16 AM | |
Joined: 3/25/2008 Last visit: 9/15/2025 Posts: 224 Rating:
|
Hi, the parameters are the same. check what goes on r2018.0 and r2018.1. what state the inputs r722 are in |
Follow us on