5/7/2020 7:34 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating:
|
Hello Henry; With Siemens automation equipment the answer to that question is generally very simple: if diagnostic LEDs are active it signifies the unit has encountered a problem that needs your attention. The only way to "inhibit" your diagnostic LEDs is to correct the fault they are pointing to (follow the link to "Error Messages" in the page below). The RF680R manual shows different ways to determine the source of he error, including a description of the diagnostic LEDs (see the screeshot below): https://support.industry.siemens.com/cs/ww/en/view/109756191/105551149707 Hope this helps, |
Last edited by: dchartier at: 05/07/2020 19:37:07Last edited by: dchartier at: 05/07/2020 19:40:30 |
|
5/7/2020 8:09 PM | |
Joined: 4/24/2014 Last visit: 8/2/2024 Posts: 4 Rating:
|
I sent the command READ_EPC_MEM without RFID tag. I received error 0xA1 on LED status bar (There is no transponder with the required EPC-ID in the transmission window). Correctly. Then I sent a RESET_READER, put the TAG into antenna field and again start READ_EPC_MEM. I received the data without errors, red LED's on the status bar and ER are flashing all the time. I don't know what else to do (except power off, it helps). Henry |
Last edited by: Irokez at: 05/08/2020 09:02:39 |
|
5/14/2020 11:21 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating:
|
Ah ok. I actually haven't experienced this bahaviour. Did you already update to the latest FW? |
5/14/2020 9:41 PM | |
Joined: 4/24/2014 Last visit: 8/2/2024 Posts: 4 Rating:
|
Yes, I have latest version 3.2.1. Firmware V3.2.1 for SIMATIC RF610R, RF615R, RF650R, RF680R, RF685R. Probably the only way to fix it is black insulating tape on the LED's and reading error codes only by PLC software ;) |
Last edited by: Irokez at: 05/14/2020 21:42:20Last edited by: Jen_Moderator at: 05/15/2020 07:30:31Optimized link. |
|
5/19/2020 11:15 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating:
|
|
12/31/2020 1:25 PM | |
Joined: 7/30/2013 Last visit: 5/23/2024 Posts: 10 Rating:
|
send Init will clear the LED's |
Follow us on