Default Header
(header konnte nicht geladen werden)
1/28/2019 5:06 AM | |
Joined: 2/11/2013 Last visit: 11/18/2021 Posts: 10 Rating: (0) |
Hi, I had a Problem with my Image on the Microbox IPC427E after Restoring it. After startup Directly I received the following errors: 1- Logical Device I210(ETHERNET) <8,0,0,> is configured as interface IF2, However, the referenced device does not exist or it has not been assigned for use by RTX 2- The RTX Ethernetcontroller on IF2 does not have an exclusive IRQ WinLC RTX cannot be started After, checking WinLC Properties @ Station Configuration, and added the assigned module I210 to IF2. I had the same Problem, After Diagnostics for I210: Test results --> All Passed .. except "Interrupt Status: Failed" Trying to Change IRQ No. with available one @ (RTX PCI Device Properties) and restart. Also, WinLC RTX (Logical Controller) isn`t starting up. I have added some Screenshots to follow up. Can you please let me know if the image itself isn`t compatible with the micro-box or Something needs to be changed for the network, i have attached the microbox Data sheet also. Thank you, Islam. Attachmentscreen shots.zip (435 Downloads) |
Thank you & Best Regards. |
|
This contribution was helpful to1 thankful Users |
Follow us on