11/27/2015 9:26 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, Go to page 148: https://support.industry.siemens.com/cs/attachments/19624874/logo_0500_en.pdf The original cable this should be: 6ED1 057-1AA00-0BA0 |
11/27/2015 9:41 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
Hello Ste39,
|
11/29/2015 5:55 PM | |
Posts: 7 Rating:
|
Hi i have clearly written in my 5th post on 11/26/2015 7:21 PM that, I have purchased the USB logo cable from ebay,(the images of my cable are attached herewith) at that time i did'nt know anything about PLCs, my project guide told me "just buy a logo plc and its programming cable" and I bought the cable first becoz logo plc was not avail. at that day. but when the cable came surfing net about its drivers i found that the new version logo8 does not require that cable, from the ashulogo8's post i came to know that even there is no port to connect the usb logo cable. Now I want to buy a logo PLC which can be programmed with my USB logo cable already bought, i have two options, option 1 : throw my USB logo cable in waste basket, as ebay is not ready to return it option 2 : do not buy the newest version of logo (i.e., logo 8) but buy an old version of Logo plc which can be programmed by using my logo cable so that my investment in logo cable will not waste. I can't throw it in waste as i bought it by my pocket money, I am therefore asking you please tell me which versions of logo plcs support my usb logo cable ------- i will buy only that logo plc which can be programmed by using my logo cable to make my logo usb cable in working and useful. My work is only a switch on/ off some motors depending upon the logic / switches ---- not require advanced dataloging or webserver etc some venders are offering me logo 0ba2 the images are also attached I am confused which PLC should i buy now ? i think any one from 0ba2 to 0ba6 pls guide me, i don't want my investment a waste thanks Attachmentimages.pdf (790 Downloads) |
11/14/2022 10:42 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Gianni7733 is split to a separate thread with the subject 6ED1052-1FB00-0BA8: Does it support modbus?. Best regards |
Follow us on