4/1/2025 1:48 PM | |
Joined: 3/21/2022 Last visit: 4/2/2025 Posts: 1 Rating:
|
Hi, i have a problem Downloading the program from LOGO Softcomfort through ethernet cable to a Logo version 8.1 . The problem is that i have to download an older version of the program (LOGO version 8.0) in a newest version of the logo and save it to the SD card. When i try to copy the program in the SDCard the download bar in the LOGO display shows that i am doing the download but when i check on the pc which files i have inside it (should be an .bin and a .dat) i dont have both but only the .bin. is there a way to copy and older version of the program on the sd card through a newer version ? |
4/1/2025 1:55 PM | |
Joined: 12/18/2014 Last visit: 4/10/2025 Posts: 35071 Rating:
|
When you transfer a program to an SD card via LSC, the program is saved in a specific file format and with the only permitted file name. The file is then called "LOGO_U_P.bin." As far as I know, a ".dat" file is not saved. |
Follow us on