1/7/2021 10:57 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, yes this is the correct example image. Did you follow the setup instructions? Which IP address does your PC have? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/9/2021 4:03 PM | |
Joined: 6/1/2015 Last visit: 5/20/2025 Posts: 5 Rating:
|
(The text is a translation of the top post in this thread.) IoT2050にご興味のある皆様へ。 IOT2040の後継であるIOT2050がリリースされました。 概要: IOT2050には2つのバージョンがあります。1つはOSなしのバージョン、もう一つはOSありのバージョンです。共にLinuxを使用するシステムになります。 どちらのバージョンもTISOC AM65x8 64ビットARMプロセッサを使用し、DisplayPortを備えています。 2つのバージョンの主な違いは次の通りです。 ■6ES7647-0BA00-0YA2(IOT2050ベーシック:OSなし) デュアルコアプロセッサ(AM6528 GP) 1 GB RAM(DDR4) eMMcなし RTC用のバッテリーなし プリインストールされたOSはありません(IOT2040のようにµSDカードにインストールする必要があります) ※この製品では、サンプルイメージをµSDカードにフラッシュして挿入し、SSH経由でインターフェイスX1P2を使用して192.168.200.1に接続する必要があります。 https://support.industry.siemens.com/tf//ww/en/posts/example-image-online/239417/?page=0&pageSize=10 ■6ES7647-0BA00-1YA2(IOT2050 Advanced:OSあり) クアッドコアプロセッサ(AM6548 HS) 2 GB RAM(DDR4) 16GB eMMc RTC用の付属バッテリー eMMcにプリインストールされたSimaticIndustrial OS 2.0(DebianベースのOSです。ライセンスを含みます。) Simatic Industrial OSの詳細については、こちらをご覧ください。 ->どちらのバージョンも、IOT2040と同様に下記のインターフェースが利用できます: ArduinoUnoインターフェース 1xRS 232/485 mPCIeスロット 2xイーサネットインターフェイス(ギガビットインターフェイス) 関連ドキュメント: ■IoT2050取扱説明書(日本語) ※準備中(2021/2リリース予定) ■IoT2050取扱説明書(英語) ■IoT2050 Setting up v1.0 日本語ドキュメント (本文は本スレッドのトップ投稿の翻訳となります。) 是非、IoT2050を手にとって見てください。
|
Last edited by: mcdb_cherry at: 01/09/2021 16:05:17Last edited by: mcdb_cherry at: 01/09/2021 16:20:22 |
|
6/1/2021 11:22 AM | |
Posts: 24 Rating:
|
Hi, Is the IOT2050 Advanced already shipped with the Industrial OS preinstalled on the eMMC? If yes, which version of the Industrial OS is it? Regards, Laura |
7/22/2021 3:39 PM | |
Joined: 6/29/2015 Last visit: 4/17/2023 Posts: 2 Rating:
|
In the meantime, the CI build # 159 (realtime, specifically) seems to be working flawlessly for me so far :) |
Follow us on