Default Header
(header konnte nicht geladen werden)
3/9/2023 5:45 AM | |
Joined: 11/19/2022 Last visit: 3/9/2023 Posts: 1 Rating:
|
Hello, First of all, I realize that it's been a long time since the problem, but I'm having the same problem right now. Do you remember how did you solve the problem? Before your answer, the points I have checked *I noticed that the ground wire was broken in the first place and I fixed the problem. But I continued to experience the same problem in the following hours. *There is no EEPROM available in the PLC system. So the problem is not with the EEPROM. *Although the system has been operating for a long time under normal conditions, it causes me to experience the same problems when I try on the spare PLC unit.
------------------------------------------------------------------------------------------ |
Last edited by: PhoenixBull at: 03/09/2023 05:47:19Last edited by: Jen_Moderator at: 03/09/2023 12:16:19New subject after splitting. Quote embedded. |
|
Follow us on