1/8/2024 8:43 AM | |
Joined: 3/2/2007 Last visit: 6/27/2024 Posts: 932 Rating:
|
Kindly, where can we find the specs of the internal braking resistor inside the V90 drives ? We need to know its maximum power (kW) and its maximum energy (kJ). 6SL3210-5FE11-0UF0, Siemens , Sinamics V90, with Profinet Input voltage: 380-480 V 3 A -15%/+10% 3.8 A 45-66 Hz Output voltage: 0 – Input 3.0 A 0-330 Hz Motor: 0.75/1.0 kW Degree of protection: IP20 Size A, 80x180x200 (WxHxD) 1FL6062-1AC61-2LA1, Siemens , Simotics S-1FL6-1FL6 Operating voltage 3AC 400 V Pn=1 kW; Nn=2000 rpm M0=6 Nm; MN=4.78 Nm Shaft height 65 mm, with angle plug; absolute encoder 20-bits (12-bit multi-turn) with feather key, tolerance N without holding brake Degree of protection IP65 with sealing ring compatible with the converters Sinamics V70 & V90 |
... thank you ... |
|
1/8/2024 2:14 PM | |
Joined: 10/11/2006 Last visit: 6/27/2024 Posts: 5869 Rating:
|
Hello Ziemens, |
With best regards, |
|
1/9/2024 7:25 AM | |
Joined: 3/2/2007 Last visit: 6/27/2024 Posts: 932 Rating:
|
The internal braking resistor has the same ohms as the recommended external one (160 Ω) ? |
... thank you ... |
|
Follow us on