Default Header
(header konnte nicht geladen werden)
5/25/2011 8:28 AM | |
Posts: 4 Rating:
|
From the session I recently attended For Sinamics Drive, there are some points which I would like to clarify and put forth to the moderators.It is learnt from the Features of Sinamics that We Provide an MMC Slot for the transfer of Code into the Sinamics Drive.Queries [schnippschnapp] We provide an USB Port for Sinamics drive. Do we have any secure protocol for accessing?? If no
Do we have any methods to find the corrupt data inside the removable device?. Do we have an Data Validation Feature when we copy the data from MMC to the Sinamics?. access and move data only if the data is Valid. |
Last edited by: O_Moderator at: 5/26/2011 11:26 AMnew subject after splitting |
|
Follow us on