Default Header
(header konnte nicht geladen werden)
3/29/2013 6:01 AM | |
Joined: 2/24/2009 Last visit: 8/20/2024 Posts: 116 Rating: (2) |
Dear Sir, We have a machine which contain S7 416 3DP PLC & 6RA 24 60 Amp drive, which is communicating to PLC over profibus. Now we want to change drive to 6 RA 80. In hardware configuration of PLC they have configured 6RA 24 with PPo 4. What hardware configuration we should select for 6RA 80. We have tried with standard telegram 352. Please send a sample program for 6RA 80 on profibus with S7 400 PLC. Wheather the logic for speed setpoint needs to change for 6RA80. We are able to read data from 6RA80 but setpoint processing is not proper. Please find attached herewith parameter list for 6RA 24.Please go through parameter and suggest care needs to be taken while configuring 6RA 80. Please do the needfull. regards, Rahul Sayr
AttachmentDrive_1.zip (342 Downloads) |
Follow us on