Default Header
(header konnte nicht geladen werden)
6/18/2014 11:00 AM | |
Joined: 8/25/2006 Last visit: 10/4/2024 Posts: 2209 Rating: (279) |
Hello. DCM from hereProfibus DP/Additional field devices/Drives/Sinamics (GSD file) is manually installed GSD-file via menu 'Options - Install GSD File'. DCM from hereProfibus DP/Sinamics/Sinamics DCM/ installed by Starter SSP. There will be no difference for communication from where you insert slave. But using slave fromProfibus DP/Sinamics/Sinamics DCM is more flexible for configuration. If I'm not mistaken red triangle means that gsd-file installed by installation of additional software, such as DriveES, Starter, and may be some else. If you need gsd for V1.4 you need to install latestStarter V4.3.3.1. GSD V1.4 also availablehere.
|
Last edited by: KSN at: 6/18/2014 11:02 AM |
|
Follow us on