Default Header
(header konnte nicht geladen werden)
7/26/2011 10:25 AM | |
Joined: 8/25/2006 Last visit: 11/6/2024 Posts: 2211 Rating: (280) |
Hello. Look at the List manual, description of fault F60031. Look at function diagram 8020, check parameters p50590, p50591, p50388, p50389, p50390 and adjust them if required. Also check the actual torque limits in parameters r52143,r52144, may be you have small limits. |
7/18/2014 5:14 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
Duplicate topic split intosinamics DCM drive take f 60031and closed. With best regards, Narrator1
|
Follow us on