Default Header
(header konnte nicht geladen werden)
12/11/2014 9:28 AM | |
Joined: 2/20/2007 Last visit: 6/11/2024 Posts: 122 Rating: (2) |
Hi, In one of the projects, we have two DC Motors of Armature Voltage 240V DC which is connected in series. So I need to supply 480V DC for these motors for series Operation from Drive. The problem here is that ,Customer has 3 phase 415 V ACSupply only. Kindly inform which drive we can select? 1) Drive with Incoming 400V AC or 2) Drive with Incoming 480V AC. Regards, Ahmed -------------- New subject after splitting from Field Voltage of 6RA80. |
Last edited by: Min_Moderator at: 12/11/2014 1:49 PMSplitted |
|
Follow us on