6/8/2023 1:48 PM | |
Posts: 1 Rating:
|
I need to replace a DC motor application with an AC motor. The DC motor is used to rotate two wheels which draws polyester fibre. The speed needs to be accurate to ensure the fibre thickness is correct. The torque required to turn the wheels is more than a fan and similar to a pump. The DC motor specs are: 2.92kW Varm 440V/ Vexc 220V 7.5/0.7A 1390RPM The operating speed, depending on product type can vary from 700-1100 RPM. Which AC motor will be suitable for this application? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/09/2023 04:33:15New subject after splitting |
|
Follow us on