Default Header
(header konnte nicht geladen werden)
6/9/2009 5:25 PM | |
Joined: 9/16/2008 Last visit: 9/7/2025 Posts: 56 Rating:
|
Hi, I'm using an CPU416-3DP and FM 458-1 DP (newer version ---0AA2). I've created a library object where blocks are in FB and FC. From that library, I want to use some of the blocks in CFC. But I'm not able to get that. Is there any way of implementing S7 Library in CFC? In CFC I'm not getting the Library nor the S7 Program element. FYI I've attached the zip file. Thanx and Regards AttachmentCFC.zip (643 Downloads) |
Follow us on