6/20/2024 9:04 AM | |
Joined: 5/30/2022 Last visit: 8/28/2025 Posts: 634 Rating:
|
Hi U_a5143c9b-b65a-48d9-ae71-e7e990950a52, What you are talking about is the maximum number of inputs and outputs supported by a single Logo as indicated in the manual: Maximum setup with expansion modules Then the Logo can communicate with other Logos (up to 8) and read/write from their inputs/outputs so it would be a way to expand: |
If this information really helps, you could use the Rate function. |
|
Follow us on