(0)| 10/16/2024 2:35 PM | |
|
Joined: 7/22/2023 Last visit: 4/30/2025 Posts: 7 Rating:
|
Hello, I have recently purchased a new Simatic DCM DC drive. I need to commission the drive with motor parameters. This drive is controlled by profibus through S7 300 PLC. I have STARTER software, the drive gets accessed but when I click on Load on PG command, it reaches 74% and fails. I am using an MPI adapter cable to operate the above. Please suggest. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/16/2024 21:19:27New subject after splitting |
|
| 10/16/2024 9:20 PM | |
|
Joined: 7/30/2024 Last visit: 12/29/2025 Posts: 1169 Rating:
|
Closed because posted twice. The active topic can be found here: Commissioning of Sinamic DCM Drive
Kind regards, Moderator_Lan |
Follow us on