10/24/2024 6:37 PM | |
Posts: 1 Rating:
|
Hi, I transformed an old washing machine with mechanical programming by installing a logo 8.3. as per photo, I made several washing programs, but every time I want to change the type of wash, I have to load it onto the logo from the PC. I was wondering if it was possible to put all the washes on an SD card and load them when needed. Thanks. ---------------------------------- Ciao, ho trasformato una vecchia lavatrice con programmazione meccanica installando un logo 8.3. come da foto, ho fatto svariati programmi di lavaggio, me tutte le volte che voglio cambiare tipo di lavaggio, devo caricarlo sul logo da pc. Chiedevo se era possibile, mettere tutti i lavaggi su scheda sd e caricarli al bisogno. Grazie. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/24/2024 21:17:22New subject after splitting |
|
10/25/2024 9:38 AM | |
Joined: 4/11/2022 Last visit: 8/26/2025 Posts: 90 Rating:
|
Sorry Mr. Smart, you are the best really! |
Rgds, |
|
10/25/2024 9:50 AM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35909 Rating:
|
And I hope you feel really good now because you gave the worst rating you could gave. |
Follow us on