(3)| 11/1/2024 9:46 AM | |
|
Joined: 6/11/2019 Last visit: 12/26/2025 Posts: 2709 Rating:
|
The problem, as I have read, is that Cn004 does not query the analog input AI1 and AI2 at all For what you have in mind, I would rather choose the Cn002 or Cn005 mode and use the Logo to determine the speed. You only need a few muxers in the program for this (see "Speed 1-8"). For emergency operation, you can use a 2-pole changeover switch that switches between the analog output module and the potentiometer. This can be implemented as a key switch. I would never give an operator access to the parameterization level of a converter. The risk is simply too great that they will change other things and damage the converter or the system. Regards Ella_68 AttachmentSpeed 1-8.zip (294 Downloads) |
Follow us on