Default Header
(header konnte nicht geladen werden)
12/16/2024 3:18 PM | |
Joined: 6/25/2024 Last visit: 8/29/2025 Posts: 10 Rating:
|
I already used that G codes initially in the program, but when I execute a program with the G codes (G81-G89), the mentioned alarm in the photo appears. For don´t use that G290 and G291 I modificated the param 20150[46] G_CODE_RESET_VALUES (is relationated with code G290 which is the "Sinumerik Mode") originally this param are with "1", and this means that G290 are active, so I changed it to "2", which means that G291 (ISO Dialect mode) is active always. |
Follow us on