1/8/2025 9:36 AM | |
Joined: 9/23/2005 Last visit: 9/2/2025 Posts: 5112 Rating:
|
First you should let us know which software you use and choose correct conference. STEP 7 (TIA Portal) or STEP 7 / STEP 7 Lite Then we would like to know hardware you use. Finally describe what is the meaning of this REAL number result (e.g. 50.0 means 50 Hz) and what is interpretation of analog output signal. Eg. 10V means for an inverter to run at 100 Hz. |
Last edited by: jacek d at: 01/08/2025 09:37:32Regards, |
|
1/11/2025 6:59 PM | |
Joined: 5/6/2010 Last visit: 8/31/2025 Posts: 2029 Rating:
|
Hello, first of all, it's easier to give you a qualified answer if you tell us
If you want to read a analog input you should know that you must convert and calculate the value of the input word. (NORM, SCALE) Please have a look at this link to handle analog values: SIMATIC S7-1500, ET 200MP, ET 200SP, ET 200AL, ET 200pro, ET 200eco PN Analog value processing Convert a DINT to a INT is "easy". If you tell us the PLC which you use, I can give to a example to do the "easy" conversion. regards |
Follow us on