Default Header
(header konnte nicht geladen werden)
(0)| 2/26/2025 7:40 AM | |
|
Joined: 2/26/2025 Last visit: 3/5/2025 Posts: 1 Rating:
|
Hello everyone, I also have a problem with a CU320-2DP board (6SL3040-1MA00-0AA0). To explain my problem, I had my original control unit (6SL3040-0MA00-0AA1) which had the two LEDs RDY and DP flashing red when starting the machine and then it goes out, impossible to start the machine. When I connect the console with SIMOTION SCOUT, the error message “Station Failure” appears for my original CU320 card. We ordered a new card with the same part number, but the supplier delivered a replacement because the original card is obsolete. I installed the new card using the same address as the original, inserted the original CF card, and upgraded the device version using SIMOTION SCOUT -> Target device. This is when my problem appears. The following error message appears: “Error establishing connection with device SINAMICS_S120_CU320-2DP”. “Check your interface parameters! (ref : 0xbe0b0028) The LEDs on the CU320-2DP unit are RDY orange and DP flashing red. Can you help me with this replacement? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: bauwin_seb_066 at: 02/26/2025 07:41:49Last edited by: Moderator_Lan at: 02/26/2025 08:35:52New subject after splitting |
|
Follow us on