3/12/2025 10:33 AM | |
Joined: 10/3/2023 Last visit: 8/20/2025 Posts: 53 Rating:
|
Hi Experts, I have an Simatic IPC477E (6AV7241-3DA07-0FA0). This Unit not Booting and showing "Recovery Your Computer or device needs repair". i tried so many times but still this screen only showing. Also, If i press ESC button it's going to the boot settings but all options have password. I don't know what the password is!. I'll Attach photos for the reference. Kindly, help me to get the solution. Thank you AttachmentNew folder.zip (188 Downloads) |
3/12/2025 12:26 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Riyasa, In this case, when you get this type of error, you need to perform a restore of the IPC. To restore/format the IPC, you must do so using the DVD/USB that comes with the IPC, as explained in the following FAQ: I recommend that you try installing it in UEFI Mode, not Legacy Mode. Could you try this restore and let me know the result?
|
If this Information really helps, you could use the Rate function |
|
Follow us on