3/19/2025 12:43 PM | |
Joined: 10/10/2018 Last visit: 3/26/2025 Posts: 6 Rating:
|
Dear users, I have a project with TIA Portal V15 where we use ReportPrinter to print an OnlineTrendControl object. It works, the image is sharp, and the text on the axis is the correct size. I upgraded the project to TIA Portal V18 without making any changes, but the image quality decreased (images attached). If I change the OnlineTrendControl size in RT and match it to the size specified in ReportPrinter, the image appears correctly. However, this option is not valid for me because it doesn't match the screen size. Do you have any idea what might be happening? It's as if it prints the image and it doesn't scale when printing. Thank you very much!
AttachmentPrint_OnlineTrendControl.pdf (175 Downloads) |
Last edited by: Mprat at: 03/20/2025 10:08:16 |
|
3/21/2025 9:56 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello Mprat Do you use the latest Update for your TIA V18 and the WinCC RT Professional installation? https://support.industry.siemens.com/cs/de/en/view/109817218 Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/26/2025 10:36 AM | |
Joined: 10/10/2018 Last visit: 3/26/2025 Posts: 6 Rating:
|
Hello Murof, I installed the update 5 and it still doesn't work. Thank you. |
Follow us on