3/27/2025 3:33 PM | |
Joined: 4/6/2021 Last visit: 6/10/2025 Posts: 1 Rating:
|
Hello, I am trying to connect a VirtualMachine1 (with UnifiedRtUp3 installed) as UmcAgent to another VirtualMachine2 that is a UmcRingServer (with TiaPortalV19up3 installed) but a error message appear. But a don't know what ports should be open. Do you know what port should be open ? The procedure i used is below (these are my notes and it is in french) and is there something missing ? The procedure : Description : Ce document permet de configurer un UmcAgent (en bleu) au UmcRingServer déjà configuré (en orange). Il est nécessaire de créer un UmcAgent afin d’importer les GlobalUsers (résident sur vscadaspl) dans le projet TiaPortal (résident sur vscadaing) . L’architecture de la ville est celle-ci : Références :
Procédure :
|
3/27/2025 3:43 PM | |
Joined: 7/30/2024 Last visit: 9/15/2025 Posts: 952 Rating:
|
Hello AutoGen_8599399, Please try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help to generate more replies to your question. This is the translation the french part of your post (via google translate):
Kind regards, Moderator_Lan |
Follow us on