3/27/2025 9:04 AM | |
Joined: 12/20/2023 Last visit: 9/9/2025 Posts: 6 Rating:
|
Hi, This week I also had same issue as described above. During compilation of HMI changes (TIA v16, last updates, Win 11 IoT Enterprise, last update) I received same general error without pointing at the reason. "LinkerScreen.PreLinkInstance(): cannot get all SliderWindows" I must admit, there are no pop-up screens or slide-in screens in my HMI program, I use only Global Screen to display some HMI Discrete Alarms. That works on other stations without any issue, same TIA v16 What is the case here? PS. on December I had similar issues with TIA v15.1 (HMI) on the same PG device; it was the Windows update that didn't wotk with old TIA anymore. But the message there was different "General Error. Please contact Siemens support". Is it the same issue here? Or it is linked to something different? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/27/2025 10:09:14New subject after splitting |
|
3/28/2025 2:19 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello mariusz_kiczka Does this occur only with one specific project or also with another one or a new testproject? Try this with your project if it only appears with this one: https://support.industry.siemens.com/cs/de/en/view/109778709 Then try again. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on