3/17/2025 12:32 PM | |
Joined: 2/1/2010 Last visit: 9/19/2025 Posts: 214 Rating:
|
The 2020 Advisor tool found here Determination of suitable hardware for the Process Historian with the "PH-HWAdvisor" tool as of today's date can go back to 9.0 SP3. If you check the compatibility tables of 8.2 (assuming 8.2 SP1) and 9.0 SP3 the Process Historian versions are the same. So just use the tool as if 9.0.3 for your results. Highly recommend using PH2014 SP3 Up6 which is the last / highest version. If you are stuck at 8.2 SP0 then highest compat table shows Up3, but I would tend to believe this is lack of Siemens testing due to out of data version, not that Up6 won't work. |
If my post helped you, please rate. Thanks. |
|
Follow us on