4/14/2025 12:37 PM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6018 Rating:
|
Dear mehranIII, by setting G1_STW.13 =1 (Request value cyclic transfer of the absolute position value in Gn_XIST2) the absolute value will be transferred cyclic into Gn_XIST2. The G1_STW is located in PZD5 of telegram 3. In G1_ZSW.13 it is possible to read out that the absolute position value is transferred cyclic. Please find this information in detail in the operating instructions (chapter 8.3/8.4) of the V90 under the following link: https://support.industry.siemens.com/cs/de/en/view/109824516 |
Last edited by: Wit_Moderator at: 04/15/2025 08:07:21Link optimized With best regards, |
|
This contribution was helpful to
1 thankful Users |
4/15/2025 6:24 AM | |
Joined: 12/26/2021 Last visit: 6/7/2025 Posts: 9 Rating:
|
Thanks for your reply "Technology Team" I set this value G1_STW.13 =1, but the value of G1_XIST2 is still zero. Can this setting in G1_STW.13 be applied to any position in the axis, or does it have special conditions? This value that is transferred to G1_XIST2 is the current position of the axis? I have no idea about this position, is it possible to have the value of the axis position in homing as an absolute value in the program?
With regards |
Last edited by: mehranlll at: 04/15/2025 06:28:01Last edited by: Wit_Moderator at: 04/15/2025 08:08:15Link optimized |
|
Follow us on