5/2/2025 3:23 PM | |
Joined: 3/15/2011 Last visit: 8/7/2025 Posts: 1 Rating:
|
I have a similar issue with a V16 upd6 advanced project.... I have two io-fields setup nearly identically, both calling scripts on activate and input finished. activate - script1 input finished - script2, script1, script3 One io field works perfect and the other doesn't - it seems to not run script1 on either event. If I duplicate the io-fields the duplicates behave identically to the originals. The project has hundreds of input fields to test and repair. Is there any explanation why they could behave differently? script1 - reads tag value from array script2 - wait delay script3 - creates string from data values from the two script1 calls I've tried rebuild all as the often fixes the unexplainable... ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 05/05/2025 06:20:39New subject after splitting |
|
5/6/2025 8:56 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Dkostell Do you have tried to generate all fresh: https://support.industry.siemens.com/cs/de/en/view/109778709 check also the tab sequence in the screens, because if case of entering the screen you can define which element can have the focus (run the ativate) bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on