5/13/2025 5:18 AM | |
Joined: 5/4/2023 Last visit: 5/20/2025 Posts: 2 Rating:
|
Good morning, I have a problem with PCS7 V10.0. When I have done a scada compile and want to download changes, I get all kinds of messages like 'Data Manager; Data record still exists, Data record not saved (Further information: Object=5573375, Data=, Enum=10, Notify=0, hr=8004620B, hrCommon=80046208)' (See attachment). Then I can no longer download the changes and I am forced to do a full download. I did not have this in V9.1. Can someone explain to me what these messages mean and how I can possibly solve this? Setup: 12 OS Clients, 2 ES stations, 2 OS Servers. 2 Domain controllers. AttachmentScadaDownloadFail08052025.txt (72 Downloads) |
Last edited by: Moderator_Lan at: 05/13/2025 07:47:19Attachment added |
|
5/13/2025 8:32 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Did you take the OS project online on the ES? Maybe this could be the problem, see the following FAQ: What should you do if the OS server project is taken online by mistake on the ES Also try a full OS compile with memory reset and check if changes can be done afterwards when both servers have been downloaded.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on