5/19/2025 2:37 PM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Hi, Are you sure nothing has changed since then? Commands are not changed? There is one rule for SFC: if no commands with initialization are present, the Initialization phase is not executed. Can you verify this? I have my number of shares with the EMT/EPHT and it could be well be a bug, but you need to be sure since providing this to support will take up a lot of time too. Maybe you can also add a new condition to the If statement for example a bool which you can manipulate on the front (set as link parameter). Check if the function works if you change the signal. Also, please read through the readme notes of the CFC or PCS7 V10 SP1 manuals to see if there are restrictions. If that all looks good, I suggest you create a SR |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on