10/24/2024 5:34 AM | |
Joined: 9/12/2024 Last visit: 8/18/2025 Posts: 1 Rating:
|
It is not helpful. would you please suggest any way? |
10/24/2024 9:54 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello I had today a similar issue. The reset does not help. I installed SQL Server management Studio and connect to the WInCC SQL Server instance. Then I could see in the connected databases that there are some attached WinCC databases (I had closed everything already) -> after detaching the connections everything works again. There is a FAQ for WinCC with this issue, -< its the same system as in WinCC Professional perhaps it helps: https://support.industry.siemens.com/cs/de/en/view/109818900 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
Follow us on