Default Header
(header konnte nicht geladen werden)
7/31/2006 6:41 AM | |
Posts: 10 Rating:
|
Hi All ! Please answer me this question : Can I use IM308C to connect CPU S5 115U with CPU S7 315 2DP via Profibus network ? Thanks and best Regards ! |
7/31/2006 8:53 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello enwru, Yes it's possible. See also following links: http://support.automation.siemens.com/WW/view/en/6709721 http://support.automation.siemens.com/WW/view/en/6556876 Hope this will help you, Best regards, Wizard |
7/31/2006 7:54 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="enwru"]Can I use IM308C to connect CPU S5 115U with CPU S7 315 2DP via Profibus network ? Hi Enwru, For sure that is possible! You have to decide if you want the IM 308C Slave or Master or both, the CPU 315-2DP can be Master or Slave. Because you have to do in STEP5, STEP7 and in COM PROFIBUS some things, it is very good when you work secure... [:P] To do this please, please, please do first one byte from the S5 to S7 and when that works you may do some more. [:o] The GSD-files for the S7 CPU can be downloaded from the next link: PROFIBUS GSD files : SIMATIC, after that you can use the examples that are on Internet... [;)] Good Luck |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on