3/29/2011 9:33 AM | |
Joined: 5/12/2006 Last visit: 9/18/2025 Posts: 22710 Rating:
|
Hello, have you set option "PG/PC is only master" in the sewttings auf the Adapter? Regards Christoph |
3/30/2011 12:13 PM | |
Joined: 5/12/2006 Last visit: 9/18/2025 Posts: 22710 Rating:
|
Hello, is the CU310 run up correctly? The RDY LED must be green after startup. Regards Christoph |
3/30/2011 12:38 PM | |
Joined: 8/2/2010 Last visit: 6/25/2025 Posts: 45 Rating:
|
Yes RDY LED is green. If I chang the parameters through BOP20 it correctly saved the parameters Thanks & Regards |
3/30/2011 1:18 PM | |
Joined: 5/12/2006 Last visit: 9/18/2025 Posts: 22710 Rating:
|
Hi, can you control the CU- parameter r0963 via BOP20? Which value have thisd parameter? Regards Christoph |
Follow us on