Default Header
(header konnte nicht geladen werden)
6/4/2011 8:30 PM | |
Joined: 2/20/2007 Last visit: 11/19/2024 Posts: 122 Rating:
|
Hello, Using BICO Data set you can rotate the drive via three commands. Regards, Ahmed |
6/6/2011 9:26 AM | |
Joined: 9/18/2006 Last visit: 5/31/2025 Posts: 596 Rating:
|
Hi. Parameters determine the choice of the control through the Profibus or AOP. This is probably themain problem . Quickly I can not make your option. I will propose his own version. I am using the element Switch to switch the engine speed. Hopefully this will help you. Best regards. AttachmentTwo variants speed.pdf (667 Downloads) |
Follow us on