Default Header
(header konnte nicht geladen werden)
9/23/2005 2:04 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating:
|
You wrote: >> Now I need use OPC A&E and OPC HDA function under PCS7 >> V6.0/SP2&SP3, what version's Connectivity Pack should I >> order? The more important is: Does it still could be >> ordered now? If couldn't then what's the solution? You can order the Connectivity Pack V66.0 SP1 which is released for PCS7 V6.0 SP3. I have attached you the link for more information. ==>> http://support.automation.siemens.com/WW/view/en/19077617 Best Regards Technical Support |
Follow us on