Default Header
(header konnte nicht geladen werden)
3/6/2011 2:48 PM | |
Posts: 1 Rating:
|
Hollo,every master of TDC, I want to ask a question about how to use a universal module in TDC rack. Would you like a me a example? Thank you very much! |
3/9/2011 6:38 AM | |
Joined: 8/25/2006 Last visit: 9/12/2025 Posts: 2218 Rating:
|
Hello. If you mean universal module SB590 in HW-catalog of TDC, I think this module is used for configuring VME-bus modules of third-party manufactures. The only example I know is ibaLink-SM-128V-i-2o from iba AG, which may be used in TDC-rack and configured in HW-Config as universal module SB590. May be some departments of Siemens also produce special VME-bus modules forown applications. You may read about VME-bus here. |
This contribution was helpful to
1 thankful Users |
Follow us on