Default Header
(header konnte nicht geladen werden)
5/11/2012 10:54 AM | |
Posts: 22 Rating:
|
Purchased the WinCC V11 RT Adv license(2048 power tags). Installed it to PC. During the installation, only WinCC RT Adv and License Manager have been chosen to install, excluding additioanl apps. After the installation launch the Automation License Manager, transferred the license from usb stick to hard drive. Launched RT. After 15 seconds there is window with message "License Key nicht verfugbar! WinCC Audit for Runtime Advanced". Window shown 2 sec, appears, then popup the message with a list of SW(in attachements). Go again in License manager, view the list "Licensed software" - there only 1 position = WinCC V11 Pro Adv, entering to "Missing license keys" - there are 4 positions: 1. WinCC Sm@rt Server for RT Adv 2. WinCC Recipes for RT Adv 3. WinCC Logging for RT Adv 4. WinCC Audit for RT Adv What is all of that ? When i`d bought the SW, there`s wasn`t any word from siemens managers about that additional software. Is all of that SW the part of WinCC RT Adv ? How can i uninstall/delete them? Will it work correctly after deletion ?
AttachmentAttachement.zip (894 Downloads) |
Follow us on