Default Header
(header konnte nicht geladen werden)
8/19/2012 1:30 PM | |
Posts: 33 Rating:
|
Hi, Can anyone give me a method to activate runtime screen according to the plc memory bit? ex. for %M0.0 = true then Screen1 & %M0.1= true the Screen2 Thanks. |
8/20/2012 12:17 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello Perhaps the following links might help: how do you configure screen selection on a Windows-based operator panel with WinCC flexible via controller job 51? like fbelic mentioned. Or another way is: how can you make a screen selection on a Windows-based operator panel via the controller without using a controller job? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on