9/2/2008 9:22 PM | |
Posts: 75 Rating:
|
A nice tool to look into old SIMADYN files. Just unpack, no installation required. Attachmentstrucview.zip (1364 Downloads) |
This contribution was helpful to
1 thankful Users |
10/23/2008 5:58 PM | |
Posts: 1 Rating:
|
This is a newer version than the one posted by Kampf-Pasman. This was given to me by the author, Mr. Juergen Trautwig. Mr. Trautwig unfortunately has died, so there is no longer any support or program development for Strucview. He did have more recent versions, up to "j", I believe, but he was not allowed to release them to the public, as they included online access to Simadyn-D controllers, something that Siemens prohibited him from doing (he was an employee of Siemens who developed Strucview on his own time). Since Simadyn-D and Struc-G is now unsupported, I suppose Siemens would allow the online versionto be distributed, to assist in deploying newer Siemens replacement technologies.So if somebody has a newer version than this one, please post it and let me know. Thanks, Jerry Lavoie Attachmentstrucview_0.3d.zip (1424 Downloads) |
This contribution was helpful to
1 thankful Users |
10/6/2009 9:22 PM | |
Posts: 3 Rating:
|
Sushant, Regretfully, I do not have a newer version. I also do not know anybody who has it. As Juergen had explained to me, the menu structure of the version I posted shows all of the (then) currently-developed options, even those that were disabled in that release. So the online option is not useable, but is included as a grayed-out option to show that it is available in the restricted version. He told me that his superiors at Siemens disallowed him to release that version outside of Siemens. My understanding is that he also did not release it within Siemens; or if he did it was to a very limited number of persons. It is therefore unlikely that this version is able to be acquired. |
10/12/2012 6:34 PM | |
Joined: 11/26/2007 Last visit: 7/22/2025 Posts: 5 Rating:
|
It's very useful tool. |
Follow us on