Default Header
(header konnte nicht geladen werden)
11/21/2012 7:35 AM | |
Posts: 1 Rating:
|
Hello As a follow up to this discusssion I was wondering if it is now possible to migrate WinCC 7.0 SP2 to TIA v11. My specific issue: WinCC project created in 7.0 SP3. I have a comfort panel TP1500 on which i need to show these screens. The path i have tried to follow is to convert to WinCC 7.0 SP2 --> Use Migration Tool V11 SP2 UPDATE 4 ( to convert to .am11 format) and finally Use the migrate project option in TIA V11 to open the project, add the TP1500 hmi device and load the project to the HMI through ethernet. I am currently facing an error on the migration tool which does not convert the project. Any help would be appreciated. Thanks and Regards Ali PS: for reference i found that there was a training conducted on the same topic last year. If anyone who has attended this training can give more insight onto this? http://www.industry.siemens.co.uk/home/uk/en/IADT/events/listing/Documents/WinCC%20V7%20to%20V11%20Flyer.pdf
AttachmentWinCC V7 to V11 Flyer.pdf (1053 Downloads) |
Last edited by: O_Moderator at: 11/21/2012 11:16 AMquotation added Last edited by: O_Moderator at: 11/21/2012 11:15 AMnew subject after splitting from /tf/WW/en/Posts/63733#top |
|
11/21/2012 2:09 PM | |
Posts: 3037 Rating:
|
Hello, You find more information to migartion to WinCC V11 in this link. Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)? Tweety |
Follow us on