Default Header
(header konnte nicht geladen werden)
11/28/2012 12:46 PM | |
Posts: 3037 Rating:
|
Hello, You can integrate your panel in a local Network. Then you enable sharing for a folder or drive on the PC See Point 2 in following link. How do you integrate an HMI operator panel into a local network? Now you can use the function "dir" in a script and check if you can access to the shared folder on your pc.. I found an old link of ProTool of this. checking the Ethernet connection with WinCE panels (except the 170 series) Tweety |
Follow us on