Default Header
(header konnte nicht geladen werden)
1/28/2013 7:48 AM | |
Joined: 3/25/2012 Last visit: 12/23/2024 Posts: 40 Rating:
|
I don't find some options in tia portal wincc v11 like there are no script icon in the menu,there are no button enable and disable in the options of buttons,and also cann't activate selection of pc station as adevice i want to now the reasons,if it because: i setup the tia portal before winccflexible sp8 ? or becuase the licence i have is not permit these optoins ? (i setup the licence which come with the tiaportal software which i downloaded from the internet. or becuase the wincc v11 don't have these options riginally? Attachmentimg.zip (644 Downloads) |
1/28/2013 2:30 PM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Hello MINTROIN, I beleive that you got this WinCC Basic v11 as a part of STEP 7 Basic v11. In this case, sadly you don't have a PowerPack to make this WinCC Basic v11 to WinCC Comfort or above. Scripts again is not available for all devices under WinCC Comfort v11 / WinCC Advanced v11 / WinCC Professional v11. Find the devices which supports script from here - What are the functional differences between the different SIMATIC panels? You need either of the below products to make use of scripts. SIMATIC WinCC Comfort V11 SP2 - 6AV2101-0AA01-0AA5 SIMATIC WinCC Advanced V11 SP2 - 6AV2102-0AA01-0AA5 SIMATIC WinCC Professional 512 PowerTags V11 SP2 - 6AV2103-0DA01-0AA5 SIMATIC WinCC Professional 4096 PowerTags V11 SP2 - 6AV2103-0HA01-0AA5 SIMATIC WinCC Professional max. PowerTags V11 SP2 - 6AV2103-0XA01-0AA5 |
Like it? Rate it! |
|
Follow us on